The libraries in the String Libraries package can be used to process strings which
are UTF-8 encoded. The basis is the IString interface from the String Segments library. Using this interface, the strings can be passed to the respective functions
by reference. For example, to create an IString instance, the GSB.UTF8String function block from the Generic String Base library is provided.
|
String Segments |
Base functions for IString instances. |
|
String Builder |
Efficient management of UTF-8 encoded string segments. |
|
String Conversions |
Conversion of strings of different encoding to/from UTF-8. |
|
String Functions |
Functions for processing UTF-8 encoded strings following the example of the conventional standard library. |
|
Unicode Support |
Functions for processing UNICODE character categories. |
|
UTF-16 Encoding Support |
Base function for handling UTF-16 encoded memory areas. |
|
UTF-8 Encoding Support |
Base function for handling UTF-8 encoded memory areas. |
|
Generic String Base |
Function blocks for processing UTF-8 encoded strings which manage their memory statically via “GENERIC CONSTANT”. |
StringUtils library
With the help of the StringUtils library, strings in the AC500 PLC application can be handled and modified. How to use the available functions is demonstrated in the application example ⮫ StringUtils library.
-
Advantages of the new string libraries
-
Disadvantages of the established STRING functions
-
Using the IString interface